Example: Templates
Private Sub SaveMyTemplate() Trend1.SaveTemplate "Basic" End Sub Private Sub LoadMyTemplate() With Trend1 ' Set the template options to load .TemplateLoadOptions1 = _ rstTemplateLineColor Or _ rstTemplateXAxisGridColor Or _ rstTemplateYAxisGridColor Or _ rstTemplateDisplayBackground ' Could also use ' .TemplateLoadOptions1 = &H10820000& .TemplateLoadOptions2 = _ rstTemplateCustomColors Or _ rstTemplateFontInformation Or _ rstTemplateFontSize .LoadTemplate "Basic" End With End Sub
Provide Feedback