Example: DisplayMinMax property

Private Sub ToggleMinMax() If Trend1.DisplayMinMax = True Then Trend1.DisplayMinMax = False Else Trend1.DisplayMinMax = True End If ' The min/max is shown in the line legend, so if the line legend is not shown, ' the DisplayMinMax property has no effect. Trend1.DisplayLineLegend = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal