Example: ChartRadix property

Private Sub RandomRadix() Dim r As RSTradixOptions Select Case Int(Rnd * 3) Case 0 Trend1.Radix = rstRadixDecimal Case 1 Trend1.Radix = rstRadixHex Case 2 Trend1.Radix = rstRadixOctal End Select r = Trend1.Radix Select Case r Case rstRadixDecimal MsgBox "Decimal" Case rstRadixHex MsgBox "Hex" Case rstRadixOctal MsgBox "Octal" End Select ' Show some of the affected numbers Trend1.DisplayLineLegend = True Trend1.DisplayMinMax = True Trend1.DisplayPenValues = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal