Example: Scroll & ScrollMechanism properties

This example sets the chart to allow automatic scrolling during runtime and displays and hides the scrolling mechanism (VCR-style buttons) on a chart.
Private Sub ToggleDisplayScrollMechanism() If Trend1.DisplayScrollMechanism = True Then ' The scroll mechanism is shown, so hide it. Trend1.DisplayScrollMechanism = False If Trend1.Scroll = False Then ' Apparently, the operator used the VCR buttons, ' which stops scrolling. ' Start scrolling back up. Trend1.Scroll = True End If Else ' The scroll mechanism is hidden, so show it. Trend1.DisplayScrollMechanism = True End If End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal