Example: LineLegendPosition property

Sub SetLineLegend() ' If the line legend is positioned on the bottom of the chart ' then show only 4 rows, starting with the first row If Trend1.LineLegendPosition = rstLineLegendPositionBottom Then Trend1.LineLegendMaxRowsVisible = 4 Trend.LineLegendFirstVisibleRow = 1 End If End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal