DisplayScrollMechanism property
Returns or sets whether a mechanism to allow manual scrolling displays with the chart. Read/write. Boolean.
Use the ScrollMechanism property to set the type of scrolling mechanism. Currently, VCR-style buttons are the only scrolling mechanism available.
Syntax
Trend
.DisplayScrollMechanism
[ = state
]where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.state
- is a parameter of the type Boolean that can be set to one of the following:- True. Display mechanism for scrolling.
- False. Do not display mechanism for scrolling.
Chart example

Provide Feedback