DeleteSnapshot method
Deletes the snapshot with the specified name.
Syntax
Trend
.DeleteSnapshot
(SnapshotName
)where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.SnapshotName
- is a parameter of the type String that specifies the name of the snapshot.Provide Feedback