PenConfigChanged event

This event occurs when a pen is added to, removed from, or modified on a trend chart.
Syntax
Trend
_
PenConfigChanged
(
ByVal
Change
As rstpenConfigChanges
,
ByVal
pen
As Long
)
where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.
Change
- is a constant of the type RSTpenConfigChanges that indicates what change occurred.
pen
- is a parameter of the type Long that specifies the name of the pen that was added, modified, or removed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal