Item method for Overlays collection
Returns an Overlay object specified by the Item parameter.
The value of Item can be between 1 and Count, inclusive.
Syntax
Overlays
.Item
(Item
)where
overlays -
is the name of an Overlays collection or an expression that evaluates to an Overlays collection.Item
- is a parameter of the type Variant that specifies the overlay to be returned. The value of Index can be between 1 and Count, inclusive.Provide Feedback