Add method of Overlays collection

Creates a new overlay from the specified snapshot, adds it to the Overlays collection and returns the newly created Overlay object. Defaults are used for the new overlay.
Syntax
Set
oOverlay = Overlays
.
Add
(
SnapshotName
)
As Overlay
where
overlays -
is the name of an Overlays collection or an expression that evaluates to an Overlays collection.
SnapshotName
- is the name of the snapshot that will be used to create the overlay.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal