RSTtimeSpanTimeValue constants

Sets the time span based on seconds. Use with the TimeSpan property.
The following constants are defined:
Constant
Description
rsttsDays
Seconds per day.
rsttsHours
Seconds per hour.
rsttsMinutes
Seconds per minute.
rsttsSeconds
Seconds per second. This constant is used only as a multiplier. Use this constant in the rare case that you want to determine the multiplier when setting the time span.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal