RSTtimeFormat constants

Use these constants with the TimeFormat property.
The following constants are defined:
Constant
Description
rstTimeFormat12Hour
All times display in AM / PM format.
rstTimeFormat24Hour
All times display in 24-hour format.
rstTimeFormatSystem
All times displayed in system format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal