RSTscrollModes constants

Use the constants with the ScrollMode property.
The following constants are defined:
Constant
Description
rstContinuousScroll
The chart scrolls from the right to the left for each new data reading.
rstHalfScreenScroll
The chart scrolls a half screen at a time, from right to left.
rstFullScreenScroll
The chart scrolls a full screen at a time. Pens scroll from the left to the right, starting at the left-most side of the screen. When the pens reach the right side of the screen, the entire screen scrolls and the pens scroll again, beginning at the left side. Use this scrolling option with overlays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal