RSTscrollDirection constants

Use these constants with the ScrollClient method.
The following constants are defined:
Constant
Description
rstScrollDirectionBeginHistData
Sets the start time of the viewer to the oldest data.
rstScrollDirectionFullScreenBack
Subtracts one time span from the start time.
rstScrollDirectionHalfScreenBack
Subtracts half of a time span from the start time.
rstScrollDirectionHalfScreenForward
Adds half of a time span to the start time.
rstScrollDirectionFullScreenForward
Adds one time span to the start time.
rstScrollDirectionEndHistData
Sets the start time of the viewer to the newest data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal