RSTruntimeAttributesEnabled constants
Use these constants with the RuntimeAttributesEnabled property to specify which features are available at runtime.
The following constants are defined:
Constant | Value | Description |
---|---|---|
rstEnableAll | Enables all options. | |
rstEnableNone | Disables all options. | |
rstEnableChartPage | 0x00000001 | Allows runtime access to the General property tab. |
rstEnableXAxisPage | 0x00000002 | Allows runtime access to the X-Axis property tab. |
rstEnableTemplatePage | 0x00000004 | Allows runtime access to the Template property tab. |
rstEnableOptionsPage | 0x00000009 | Allows runtime access to the Display property tab. |
rstEnablePensPage | 0x00000010 | Allows runtime access to the Pens property tab. |
rstEnableYAxisPage | 0x00000020 | Allows runtime access to the Y-Axis property tab. |
rstEnableEditLegend | 0x00000040 | Allows runtime access to line legend line colors, pen captions, and engineering units. |
rstEnableContextMenu | 0x00000080 | Enables right-click menu on the Trend object during runtime. |
rstEnableDeltaValueBarCmd | 0x00020000 | Allows operators to use the delta value bar at runtime. |
rstEnableDragDrop | 0x00000100 | Allows operators to create pens during runtime by dragging addresses from RSLogix and dropping them on the chart. This option is not available for all containers. |
rstExecuteTrendCmd | 0x00000200 | Enables Trend. |
rstEnableScrollCmd | 0x00000400 | Enables access to scroll bars on the trend chart during runtime. |
rstEnableValueBarCmd | 0x00000800 | Allows the value bar to be displayed during runtime. |
rstEnableOverlayPage | 0x00002000 | Allows runtime access to the Overlay property tab. |
rstEnableOverlayMenu | 0x00004000 | Allows right-click access to the Overlay tab during runtime. |
rstEnableSnapshotCmd | 0x00008000 | Allows snapshots to be taken of the trend chart during runtime. |
rstEnablePrintCmd | 0x00010000 | Enables printing of trend charts during runtime. |
Provide Feedback