RSTrefreshrateTimeValues constants

Sets refresh rates based on milliseconds.
The following constants are defined:
Constant
Description
rstrrHours
Milliseconds per hour.
rstrrMilliseconds
Milliseconds per millisecond. This constant is used only as a multiplier. Use this constant in the rare case that you want to determine the multiplier when setting the time span.
rstrrMinutes
Milliseconds per minute.
rstrrSeconds
Milliseconds per second.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal