RSTpenCaptionStyles constants

The following constants are defined:
Constant
Description
rstPenCaptionStyleFullName
Displays full pen name in the line legend, including any folder names or path names, if applicable.
rstPenCaptionStyleDataItemNameOnly
Displays only the data item name in the line legend, without any folder names or path names.
rstPenCaptionStyleDescription
Displays the pen description in the line legend.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal