RSTdataPointConnections constants

The following constants are defined:
Constant
Description
rstConnected
Each point is connected to the previous point and the next point.
rstNotConnected
Points are not connected. Each point is either represented by a marker or not shown.
rstShowDiscontinuity
Points are not connected if there is a break in the data caused by a communications error or data log stopped.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal