ShowAuthenticationDialog method
Opens the electronic signature window for the specified SignatureButton object.
The electronic signature window allows signature authentication and the operations that have been set up for a SignatureButton object, to be carried out.
Syntax
object
.ShowAuthenticationDialog
where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.Remarks
- ShowAuthenticationDialog is a blocking call. Code that follows this call in a procedure will not run until signature authentication and the related operation for the SignatureButton have been completed or cancelled, and the window is closed.
- If you do not want calls blocked when the electronic signature window is open, use the ShowAuthenticationDialogEx method, instead.
Provide Feedback