PerformerGroup property
Returns or sets the name of the Windows domain group that the person who is the Performer for the object, belongs to. Read/write.* String.
Syntax
object
.PerformerGroup
[ = string
]where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.string
– is the name of the Windows domain group that the Performer belongs to.Remarks
- This property can be blank, which indicates that the user does not have to be a member of any group.
- *When the electronic signature window is open at runtime, in other words when a signature authentication operation is taking place, this property is read-only.When the electronic signature window is not open at runtime (no signature authentication is taking place), the property is read/write.This means that you can use VBA code to make changes to the signature button properties at runtime as long as the electronic signature window is not open.
Provide Feedback