EnforceClientUser property

Returns or sets a value that enables a runtime check to verify that the Performer user name is the same as the logged-in SE Client user name. Read/write. Boolean.
Syntax
object
.
EnforceClientUser
[ =
value
]
where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.
value
– is a Boolean value that determines whether or not a runtime check will be made to ensure that the Performer user name matches the name of the user logged into the SE Client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal