DateTimeString property

Returns or sets the value that is entered or shown in the electronic signature window. Read/write. Variant.
Syntax
object
.
DateTimeString
[ =
value
]
where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.
value
– is a variant value that is shown or entered in the electronic signature window.
Remarks
  • This property is shown by following the
    short date
    and
    long time
    formats of Region and Language settings of your computer.
  • This property is used when the operation selected for the signature button is
    Set Date/Time Value
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal