ViewportHeight property

Returns the height, in pixels, of the client region inside the window that is available for all non-docked displays. Read-only. Long.
If displays are docked on the top or bottom of the window, the height of the area available for non-docked displays is reduced.
Syntax
Application
.
ViewportHeight
where
Application
– is the name of a
FactoryTalk View SE
Client Application object or an expression that evaluates to a
FactoryTalk View SE
Client Application object.
Remarks
  • Use this property to arrange displays within the main FactoryTalk View SE Client window.
  • When the window is minimized, the value returned will be 0.
  • When a display is maximized, its Width and Height are greater than its ViewportWidth and ViewportHeight because Windows automatically increases the width and height of the window to hide its borders.
  • If the region includes a horizontal scroll bar, the returned value does not include the height of the scroll bar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal