ViewOnlyMode property
Returns a value that indicates whether or not the FactoryTalk View SE Client is in View-only mode. Read-only. Boolean.
Syntax
Application
.ViewOnlyMode
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
The FactoryTalk View SE Client may be in view-only mode because of a view-only license or view-only configuration setting.
When testing the animation in displays in the Graphics editor this property always returns
false
.Provide Feedback