Version property
Returns a string containing the version of the SE Client. Read-only. String.
Syntax
Application
.Version
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
When testing the animation in displays in the Graphics editor, attempts to read this property raise an error with Err.Number equal to gfxErrorTestAnimation.
Provide Feedback