TimePeriodEnd property

Returns or sets the end date and time for the current time period. To set this property, the TimePeriodAbsoluteMode property must be set to True. Read/write. String.
Syntax
DataGrid1
.
TimePeriodEnd
[ =
value
]
where
DataGrid1
- is the name of a data grid object or an expression that evaluates to a data grid object.
value
- is a parameter of the type String. This is a date/time string such as "2016/01/01 12:00:10 PM".
Example
Private Sub SetTimePeriodEnd() DataGrid1.TimePeriodAbsoluteMode = True DataGrid1.TimePeriodEnd = "2016/01/01 09:15:10 AM" DataGrid1.RefreshData End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal