Remark property
Sets or returns the remark status of the toggle switch. Read/write. Boolean.
Syntax
object
.Remark
[ = value
]where
object
– is the name of a graphic object, or an expression that evaluates to a graphic object.value
– is a Boolean value that specifies the remark status.- True: The remark is enabled.
- False: The remark is disabled.
Provide Feedback