Quit method
Closes all windows and shuts the FactoryTalk View SE Client down.
Syntax
Application
.Quit
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
When testing the animation in displays in the Graphic Display editor, calls to this method raise an error with Err.Number equal to gfxErrorTestAnimation.
Provide Feedback