PendingWriteValue property

Returns or sets the pending value for the tag. Read/write. Variant.
Syntax
Tag
.
PendingWriteValue
[=
value
]
where
Tag
– is the name of a Tag object or an expression that evaluates to a Tag object.
value
– is a parameter of the type Variant that specifies the pending value for the tag that will be set or returned.
Remarks
  • This property can be set to vbEmpty, or can be any value for the tag.
  • When this property is not vbEmpty, its value will be written when the WritePendingValues method of the TagGroup object is called.
  • The initial value for a Tag object is vbEmpty.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal