OffLabel property

Sets or returns the label used to represent the
off
state of a digital tag. Read/write. String.
When you create a digital tag object, the default value for this property is
Off
.
Syntax
Tag
.
OffLabel
[=
String
]
where
Tag
is the name of a Tag object or an expression that evaluates to a Tag object.
String
is an optional text that describes the
off
state of a tag, such as Off, Closed, or Safe.
Remarks
  • The label can store up to 20 characters, including spaces.
  • The On and Off labels must be different.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal