Name property (Application object)
Returns the name of the application (
Display Client
). Read-only.Syntax
Application
.Name
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
When testing the animation in displays in the Graphics editor, this property returns
Graphics
.Provide Feedback