Logout method
Logs the current user off and displays the Login dialog box.
Syntax
Application
.Logout
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
When testing the animation in displays in the Graphic Display editor, calls to this method raise an error with Err.Number equal to gfxErrorTestAnimation.
Provide Feedback