Load event

Occurs when a display is loaded. The display is not visible or animating at this point.
Syntax
Display
_
Load
where
Display
– is the name of a Display object variable that was dimensioned using the WithEvents keyword or the reserved name Display.
Remarks
  • When a display is not animating, ActiveX controls will not be activated and interaction with them may be limited.
  • When a display is not animating, property writes and method calls to Graphics objects are not allowed and will cause errors to be raised.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal