LanguageName property
Returns the name of the current language for an application. Read-only. String.
This string is localized by the operating system to the language of Windows.
Syntax
Application
.LanguageName
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Provide Feedback