Item method (Elements collection)

Returns an object specified by the Index parameter. This is the default method.
Syntax
Set
oElement = Elements
.
Item
(
Index
)
where
oElement
– is the name of an Element object variable
Elements
– is the name of an Elements collection or an expression that evaluates to an Elements collection.
Index
– is a parameter of the type Variant that specifies the element to be returned. The value of Index can be between 1 and Count, inclusive, or the name of an element.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal