Elements property (Display object)
Returns a collection of Element objects contained in a display. Read-only.
Syntax
Display
.Elements
where
Display
– is the name of a Display object or an expression that evaluates to a Display object.Remarks
- The collection that is returned is hierarchical in that only objects at the root level of the display are in the collection.
- The collection can contain Group elements which in turn, are composed of collections of elements.
Provide Feedback