CurrentUserHasGroup method

Returns True if the current user is assigned to the specified user group.
Syntax
bHasGroup = Application
.
CurrentUserHasGroup
(
sGroups
)
where
bHasGroup
– is a Boolean variable that will be set to True if the current user is assigned to the specified group.
Application
– is the name of a
FactoryTalk View SE
Client Application object or an expression that evaluates to a
FactoryTalk View SE
Client Application object.
sGroups
– is a string that stands for the name of a group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal