CurrentComputerGroups property
Returns the group list that the current computer is assigned to. An empty string list is returned if the computer is not assigned to any group. Read-only. StringList.
Syntax
Application
.CurrentComputerGroups
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
In the FactoryTalk security policies, if you use the names of terminal client to identify terminal server clients, make sure to add the terminal client account to the FactoryTalk network directory. Otherwise, it cannot get the current terminal client computer name and will return errors. For more information about FactoryTalk security policies, see FactoryTalk Help.
Provide Feedback