ConfigurationFileName property

Returns the fully qualified name of the configuration file that is loaded. Read-only. String.
Syntax
Application
.
ConfigurationFileName
where
Application
– is the name of a
FactoryTalk View SE
Client Application object or an expression that evaluates to a
FactoryTalk View SE
Client Application object.
Remarks
When testing the animation in displays in the Graphics editor, attempts to read this property raise an error with Err.Number equal to gfxErrorTestAnimation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal