ApplicationName property
Returns the name of the application to which the FactoryTalk View SE Client is connected. Read-only. String.
Syntax
Application
.ApplicationName
where
Application
– is the name of a FactoryTalk View SE
Client Application object or an expression that evaluates to a FactoryTalk View SE
Client Application object.Remarks
When testing the animation in displays in the Graphics editor, this property returns the name of the application to which the display belongs.
Provide Feedback