AfterAnimationStop event
Occurs after a display stops animating. This event occurs after all elements have been deactivated.
Syntax
Display
_AfterAnimationStop
where
Display
– is the name of a Display object variable that was dimensioned using the WithEvents keyword or the reserved name Display.Remarks
- If the display is in the process of stopping and is asked to be animated again, the AfterAnimationStop event still fires.
- Calling the StartAnimation method is allowed from this event handler.
Provide Feedback