DelayInterval property

Gets or sets the will delay interval. Read/write. Double.
This property determines how long the server will delay the publication of the will message after the network connection closes, measured in seconds.
Syntax
msg
.
DelayInterval
where
msg
- is an MQTTWillMessage object.
Default value
If this property is omitted, it will use its default value, which is 0 seconds, meaning the server will immediately publish the will message when the network connection closes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal