SubscriptionIdentifiers property
Gets or sets the subscription identifiers of the application message. Read/write. Variant.
Syntax
msg
.SubscriptionIdentifiers
where
msg
- is an MQTTMessage object created by the MQTTFactory object's method CreateApplicationMessage
.
TIP:
This property's data type is Variant, however, it can only be assigned an array of integer or just a single integer. When passing an array, the last integer of the array will be used as the subscription identifier. When passing an integer, you must use the
CLng
function to convert the value to a Long data type to receive an integer. For example, msg.SubscriptionIdentifiers = CLng(
.value
)Provide Feedback