QoS property
Gets or sets the QoS level of the application message. Read/write.
Syntax
msg
.QoS
where
msg
- is an MQTTMessage object created by the MQTTFactory object's method CreateApplicationMessage
.Default value
If this property is omitted, it will use its default value, which is
MqttQoSLevel_AtMostOnce (0)
, meaning the message arrives at the receiver either once or not at all.Provide Feedback