ClientFile property

Gets or sets the client certificate file. Read/write. String.
Only client files with the
.pfx
extension are supported.
Syntax
fileCert
.
ClientFile
where
fileCert
- is an MQTTFileCertificate object.
Example
connOption.FileCertificate.ClientFile = "C:\Users\Administrator\Desktop\CA\client.pfx" ' connOption is an MQTTConnectOption object created by the MQTTFactory object's method CreateConnectOption
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal