MQTTDisconnectedEvent object
When the MQTT client disconnects from the broker, it returns the relevant information. This event is triggered when the MQTT client disconnects from the broker. The MQTT client can get the reason for disconnection through the following properties.
Properties
Provide Feedback