WithStoreCertificate method
Connects to the broker with a store certificate.
Only client certificates with the
.pfx
extension are supported.Syntax
connOption
.WithStoreCertificate
(Location
As MqttCertStoreLocation, Thumbprint
As String)where
connOption
- is an MQTTConnectOption object created by the MQTTFactory object's method CreateConnectOption
.Location
- is a constant of the MqttCertStoreLocation object.Thumbprint
- is the thumbprint of the certificate.Provide Feedback