Version property

Gets or sets the MQTT version. Read/write.
Syntax
connOption
.
Version
where
connOption
- is an MQTTConnectOption object created by the MQTTFactory object's method
CreateConnectOption
.
Default value
If this property is omitted, it will use its default value, which is
MqttVersion500
, meaning the version of the MQTT protocol is 5.0.0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal