TcpTimeout property

Gets or sets the TCP timeout. Read/write. Long.
Syntax
connOption
.
TcpTimeout
where
connOption
- is an MQTTConnectOption object created by the MQTTFactory object's method
CreateConnectOption
.
Default value
If this property is omitted, it will use its default value, which is 100 seconds. The timeout will be applied at the socket level and internal operations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal