MaximumReceiveSize property

Gets or sets the maximum number of unacknowledged PUBLISH messages the client can accommodate. Read/write. Long.
Syntax
connOption
.
MaximumReceiveSize
where
connOption
- is an MQTTConnectOption object created by the MQTTFactory object's method
CreateConnectOption
.
Default value
If this property is omitted, it will use its default value, which is 65,535.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal